:CALibrate:MODule:SLOT:STATus:TEMPerature?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:STATus:DTEMperature? command.
Query Syntax
:CALibrate:MODule:{SLOT{1:8} | LMODule | RMODule}:STATus:TEMPerature?
Description
Queries the N1000A's change in temperature from the time when the last vertical calibration and precision timebase/clock recovery calibration was performed. A calibration should be performed if the change in the N1000A's temperature exceeds ±5°C. Use the :CALibrate:MODule:SLOT<N>:STARt command to start a calibration.
Example Returned Status String
"-6.10"
Example Command
:CALibrate:VERTical:SLOT1:STATus:TEMPerature?