:CALibrate:VERTical:SLOT:STATus:TEMPerature?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:VERTical:STATus:DTEMperature? command.
Query Syntax
:CALibrate:VERTical:{SLOT{1:8} | LMODule | RMODule}:STATus:TEMPerature?
Description
Queries the change in the N1000A's temperature from the time when the last electrical or optical vertical channel calibration was performed on the indicated module. A calibration should be performed if the change in N1000A temperature exceeds ±5°C. Use the :CALibrate:VERTical:SLOT<N>:STARt command to start a vertical calibration.
Example Returned Status String
"-6.10"
Example Command
:CALibrate:VERTical:SLOT3:STATus:TEMPerature?