:CALibrate:FRAMe:STATus?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.03.00 and above, use the :CALibrate:FRAMe:TIMebase:STATus command. To return the status of the calibration for the N1000A's internal precision timebase, use the :CALibrate:FRAMe:PTIMebase:STATus command.
Query Syntax
:CALibrate:FRAMe:STATus?
Description
Queries the status of N1000A frame calibration. One of the following response strings is returned:
- "CALIBRATED"
- The N1000A does not require a calibration.
- "UNCALIBRATED"
- The N1000A requires a calibration.
Use the child queries listed in the following table to return details about the current calibration.
| Status Sring | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Temperature change since last calibration |
:DETails?
|
| Change in temperature | :DTEMperature?
|
| Change in Time | :TIME?
|
Requires FlexDCA revision A.02.00 and above.