:CALibrate:VERTical:SLOT:STATus:DETails?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:VERTical:STATus:DETails? command.
Query Syntax
:CALibrate:VERTical:{SLOT{1:8} | LMODule | RMODule}:STATus:DETails?
Description
Queries a string that lists the following calibration status information for a dual electrical, dual optical, or optical/electrical module. Modules are identified as being installed in either :SLOT1 or :SLOT3.
- Time of last calibration
- Time change since the last calibration
- Temperature change since last calibration
Example Returned Status String
"Time of last Calibration: 12/28/2011 08:14:02,Elapsed Calibration Time: 1 minutes,Temperature Change: -0.50°C"
Example Command
:CALibrate:VERTical:SLOT3:STATus:DETails?