:DISK:DWIZard:FNAMe
Command Syntax
:DISK:DWIZard:FNAMe "<path substitution string>\subfolder\filename"
Where:
- "<path substitution string> is a string that expands into a specific file path.
- "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\Documentation Results.
- "filename" is a string without the filename extension.
Query Syntax
:DISK:DWIZard:FNAMe?
Description
Specifies the filename, path, and extension for a Documentation Wizard zip file. To actually save the file, use the :DISK:DWIZard:SAVE command. The saved file is a ZIP (.zip) file. This command supports the DEFault common child command.
The default folder for storing Documentation Wizard files is in %USER_DATA_DIR%\Documentation Results as shown in this pictures. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\Documentation Results\filename.
File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Preset.
Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.
Example Command Sequence
:DISK:DWIZard:FNAMe "%USER_DATA_DIR%\Documentation Results\DocumentationResults_PAM4.zip" :DISK:DWIZard:SAVe;*OPC?
Requires FlexDCA/FlexRT revision A.04.50 and above.