:DISK:DWIZard:RESults:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:DWIZard:RESults:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add the results shown in the measurement Results table. The data is placed in a comma-delimited ASCII file (Results Window Results.csv). A screen capture of the Results table (Results Window Screen Capture.png) is also saved. The instrument must be in Oscilloscope or Eye/Mask mode (:SYSTem:MODE) and the Results table displayed.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:RESults:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.