:DISK:DWIZard:SSINfo
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:DISK:DWIZard:SSINfo {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add the system information that is shown in the Help > About dialog (SystemInfo.txt).
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:SSINfo?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.