:DISK:DWIZard:OJITter:SDATa
Meas. mode:
Jitter
Waveform type:
PAM4
Waveform record:
MV
Instrument:
N1000A
DCA-M
FlexDCA mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Command Syntax
:DISK:DWIZard:OJITter:SDATa {ON | OFF | 1 | 0}
Query Syntax
:DISK:DWIZard:OJITter:SDATa?
Query Response
{ON | OFF | 1 | 0}
Description
When saving a Documentation Wizard zip file (:DISK:DWIZard:SAVE), use this command to add the results for Jitter mode's 12-Edge Output Jitter measurements for PAM4 waveforms. These measurements are activated by the :MEASure:JITTer:OJITter:STATe command. The command arguments are:
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
The following two files are added to the Documentation Wizard zip file:
- An ASCII CSV file of the Output Jitter panel measurement results including table labels (Output Jitter Window Results.csv).
- A screen capture of the Output Jitter panel measurement results (Output Jitter Window Screen Capture.png), as shown in the following figure.
Requires FlexDCA revision A.05.70 and above.