:DISK:DWIZard:SSParam
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:DWIZard:SSParam {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add Touchstone S-parameter files for a TDR DUT setup (example, DUT N S-Parameters.s2p). The instrument must be in TDR mode (:SYSTem:MODE).
Touchstone files can be imported into Keysight's Physical Layer Test Systems (PLTS) for further analysis. S-parameters cannot be imported back into TDR mode. However, S-parameters can be imported into the following FlexDCA Waveform Signal Processing operators:
- Apply s2p (
:SPRocess:CONVolve:FNAMe) - Apply s4p (
:SPRocess:DCONvolve:FNAMe) - Remove s2p (
:SPRocess:DEConvolve:FNAMe) - Remove s4p (
:SPRocess:DDEConvolve:FNAMe)
These operators are used to transform measured waveforms to compensate for the effects of various test-setup devices.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:SSParam?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.