:DISK:DWIZard:T:OHMS{1:4}:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Command Syntax
:DISK:DWIZard:T:OHMS{1:4}:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add a data file for each displayed T-parameter waveform in any Time-Ohms waveform content windows. These are ASCII XY-value waveform files and one file is saved for each displayed waveform (for example, T11 Ohms.txt). A screen capture of the Time-Ohms waveform content window is also saved (Time-Ohms N Window Screen Capture.png). TDR mode (:SYSTem:MODE) must be selected.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:T:OHMS:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.05.40 and above.