:DISK:DWIZard:WAVE:IASParams
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
Command Syntax
:DISK:DWIZard:WAVE:IASParams {ON | OFF}
Query Syntax
:DISK:DWIZard:WAVE:IASParams?
Query Response
{ON | OFF}
Description
When saving Waveform Window Data to a Documentation Wizard zip file (:DWIZard:SAVE) in Oscilloscope or Eye Mode, this command allows you to include or exclude the saving of applied S-parameter files with the saved waveform file. The following command arguments are used:
ON- Includes any applied S-parameter files with the waveform file. This is the default setting.
OFF- Excludes the saving of any applied S-parameter files with the waveform file.
Requires FlexDCA revision A.07.90 and above.
Example Command
:DISK:DWIZard:WAVE:IASParams ON