:DISK:DWIZard:GDELay{1:4}:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:DWIZard:GDELay{1:4}:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add an ASCII data file (XY-value waveform file) for each displayed waveform in any GrpDelay (Group Delay) waveform content windows. GrpDelay waveform content windows display waveforms from different sources depending on the instrument mode:
- In Oscilloscope or Eye Modes: waveform source is an FFT function. Saves one waveform file for each displayed waveform (example, FFT[1A] (F1).txt)
- In TDR Mode: waveform source is S-parameters. Saves one waveform file for each displayed waveform (for example, S11 Delay.txt).
A screen capture each displayed GrpDelay waveform content window is also saved (GrpDelay N Window Screen Capture.png).
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:{1:4}GDELay:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.