:DISK:DWIZard:JGRaphs:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Command Syntax
:DISK:DWIZard:JGRaphs:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add the Jitter database file (JitterDatabase.jdx). The Jitter database file can be re-loaded into jitter memory using the :DISK:JDATabase:RECall command. A screen capture of the jitter graphs (Graphs Window Screen Capture.png) is also saved. The instrument must be in Jitter mode (:SYSTem:MODE).
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:JGRaphs:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.