:DISK:DWIZard:LLTResults:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:DWIZard:LLTResults:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add the results shown in the Limit Lines panel. The data is placed in a comma-delimited ASCII file (Limit Lines Window Results.csv). A screen capture of the Limit Lines panel (Limit Lines Window Screen Capture.png) is also saved.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:LLTResults:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.