:DISK:DWIZard:TIME{1}:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:DWIZard:TIME{1}:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add the following waveform data files associated with the Waveform content window:
- Scope Mode: ASCII XY-value waveform files (example, Channel 1A (1A).txt)
- Eye Mode: color-grade gray-scale database waveform files (example, Channel 1A (1A).cgsx)
- Jitter Mode: color-grade gray-scale database waveform files (example, Channel 1A (1A).cgsx)
- TDR Mode: ASCII XY-value waveform files for Ports (example, Port 1 (1A).txt)
For all instrument modes, a screen capture of the waveform content window is also saved (Waveform Window Screen Capture.png). The Waveform content window is the default window for viewing most waveforms.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:TIME:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.