:DISK:DWIZard:JSASpectrum:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Command Syntax
:DISK:DWIZard:JSASpectrum:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add the JSA memory database (JSA Memory.jsax). The data is placed in a comma-delimited ASCII file (Amplitude Window Results.csv). A screen capture of the jitter spectrum window (JSA Spectrum Window Screen Capture.png) is also saved. The instrument must be in Oscilloscope, Eye/Mask, or Jitter mode (:SYSTem:MODE) and with Jitter Spectrum Analysis turned on (:CRECovery:JSANalysis:ACQuire).
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
Query Syntax
:DISK:DWIZard:JSASpectrum:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.04.50 and above.