:DISK:DWIZard:JPEYe:SDATa
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Command Syntax
:DISK:DWIZard:JPEYe:SDATa {ON | OFF}
Description
When saving a Documentation Wizard zip file (:DWIZard:SAVE), use this command to add the results shown in Jitter Mode's results tables for PAM4 signals. The table's data is placed in a comma-delimited ASCII file (Eye Window Results.csv). A screen capture of the Jitter results table (Eye Window Screen Capture.png) is also saved. Jitter mode (:SYSTem:MODE) must be selected.
ON- Includes files in Documentation Wizard zip file.
OFF- Excludes files in Documentation Wizard zip file.
To save the results that are shown in the Level table for PAM4 signals, use the :DISK:DWIZard:JPLevel:SDATa command.
To save results tables for NRZ waveforms, use the :DISK:DWIZard:AMPLitude:SDATa and :DISK:DWIZard:JITTer:SDATa commands.
Query Syntax
:DISK:DWIZard:JPEYe:SDATa?
Query Response
{1 | 0}
Requires FlexDCA revision A.05.60 and above.