:DISK:DWIZard:WAVE:IINTernal
Command Syntax
:DISK:DWIZard:WAVE:IINTernal {ON | OFF}
Description
When saving Waveform Window Data to a Documentation Wizard zip file (:DWIZard:SAVE), this command adds an additional waveform file to the standard waveform file type that is already saved in the zip file. The following command arguments are used:
ON- Includes internal format waveform files in Documentation Wizard zip file. This is the default setting.
OFF- Excludes internal format waveform files from being included in Documentation Wizard zip file.
In Oscilloscope and TDT modes, an internal format waveform files (.wfmx) is added to the standard file (.txt) in the zip file. The standard file contains ASCII Y-values. The internal format waveform file is comprised of an ASCII XML header followed by binary waveform data.
In Eye/Mask mode, an internal format waveform files (.wfmx) is added to the two standard files (.csv and .cgsx). The internal format waveform file is comprised of an ASCII XML header followed by binary waveform data.
This command is not available in Jitter Mode.
Query Syntax
:DISK:DWIZard:WAVE:IINTernal?
Query Response
{1 | 0}
Requires FlexDCA revision A.05.80 and above.