:MEASure:EYE:CTDecq:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4
Command Syntax
:MEASure:EYE:CTDecq:SOURce {CHANnel{N} | DIFF{1:8}{A|C} | CGMemory{1:8} | FUNCtion{1:16} | WMEMory{1:8}}
{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.
Query Syntax
:MEASure:EYE:CTDecq:SOURce?
Query Response
<source_waveform>
Description
Selects the source waveform on which to perform the MEASure:EYE:CTDecq measurement.
Requires FlexDCA revision A.08.30 and above.