:SPRocess:TEQualizer:RPOint:IFOutput

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:RPOint:IFOutput {ON | OFF}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:TEQualizer:RPOint:IFOutput?

Query Response

{0 | 1}

Description

This is the TDECQ Equalizer operator's Infer Reference OOMA From Output setting which, by default, is ON. This is the legacy configuration which results in the Outer Optical Modulation Amplitude (OOMA) being measured on the equalizer's output where the measurement is affected by any amplification or attenuation added by the TDECQ operator.

Added for FlexDCA revision A.08.40, when this setting is OFF, the OOMA measurement is compensated to account for the operator's noise contribution. This allows a more accurate measurement on the transmitter itself.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:RRX:RPOint:IFOutput command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:RRX:RPOint:IFOutput

Requires FlexDCA revision A.08.40 and above.