<MaskYAlignMethod> Element

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ

The element's content specifies the mask's Y-axis alignment according to the eye's display or boundaries. Elements contents can be DISP or EWIN. DISP sets the alignment to the display (Vtop and Vbase). EWIN sets the alignment to the Eye Boundaries (Vone and Vzero). This element sets the Y-Axis Mask Align Measurement Area field in the Configure Measurements dialog (Measure > Configure Base Measurements > Mask Test tab).

Parent Elements

Child Elements

None.

Attributes

None.

Example

  • <MaskYAlignMethod>EWIN</MaskAlignMethod>