<Standard> Element
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ
The optional <Standard> metadata element provides the name of the standard that the mask tests against. The content is a string that is written on the Mask Test panel as shown in the following figure. The string is truncated to fit the available space on the panel. The element's contents can be empty. Although this element is optional, it is recommended that you include it in all your mask files as additional uses for this tag may be supported by future FlexDCA revisions.
Parent Elements
- <Mask>
Child Elements
None.
Attributes
None.
Example
- <Standard>Ethernet</Title>