<Mask> Element

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ

<Mask> is the root element. This element is required and is the ancestor of all other elements. This element should immediately be followed by the three metadata elements <Title>, <Standard>, and <Date> and then by the <DataRate> element as shown in the following example.

Parent Elements

None.

Child Elements

All other elements.

Attributes

None.

Example

  • <Mask>
  • <Title>10GbE 10.3125</Title>
  • <Standard>Ethernet</Title>
  • <Date>05/01/2002</Date>
  • <DataRate>1.031250e+010</DataRate>
  • </Mask>