<Setup> Element

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ

The child elements of the <Setup> element configure settings that are located in the Mask Test Scaling dialog. The child element <MaskAlignmentOptimize> does not have an equivalent dialog setting. Also, there is no element for the Configure Measurements dialog's Alignment Timing selection.

If you do not define a mask setup section in your mask file, the setup data from the last mask that was loaded will be used. This could cause unexpected or erroneous positioning of the mask.

Parent Elements

  • <Mask>

Child Elements

Attributes

None.