<MaskYTrack> Element

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ

The element's content enables or disables tracking between the Y1 and Y2 levels. Tracking ON links the y-axis scaling of the logic 0 and 1 levels. For example, if the logic 1 level increases, the logic 0 level increases by the same amount. The contents can be OFF or ON (default value).

The element sets the <MaskScaleMode> to XONLY. It also sets the Logic Levels Track setting in the Mask Test Scaling dialog (Measure > Eye/Mask Mode > Mask Test Scaling).

Parent Elements

Child Elements

None.

Attributes

None.

Example

  • <MaskYTrack>OFF</MaskYTrack>