:SOURce:CDIVide
Command Syntax
:SOURceN:CDIVide {UNITy}
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURce:CDIVide?
Query Response
{UNIT}
Description
On simulated instruments, sets the clock divide ratio.