:SOURce:SSC:FREQuency
Command Syntax
:SOURceN:SSC:FREQuency <frequency>
<frequency> is a double.
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:SSC:FREQuency?
Description
This command specifies the frequency of the modulating signal, in other words, how often the modulation cycle (from initial symbol rate to the spread frequency and back) completes.
Example Command Sequence
:SOURce1:SSC:STATe ON :SOURce1:SSC:FREQuency 33.0E+3 :SOURce1:SSC:PHASe 0.0 :SOURce1:SSC:PERCent 0.5 :SOURce1:SSC:PPM 5.0E+3 :SOURce1:SSC:PATTern TRIangle :SOURce1:SSC:STYPe DSPRead