:SOURce:SEED

Command Syntax

:SOURceN:SEED 

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:SEED?

Description

Sets or queries the seed of the random number generator used to generate the Pseudo Random pattern.

NRZ, PAM3, PAM4, and PAM6 data patterns are specified using the :SOURce:PATTern command.

The NRZ, PAM3, PAM4, or PAM6 format is selected using the :SOURce:FORMat command.

The DATA waveform type is selected using the :SOURce:WTYPe command.