:SOURce:NOISe:RN
Command Syntax
:SOURceN:NOISe:RN <RN>
<RN> is a double.
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:NOISe:RN?
Description
On simulated instruments, specifies the amount of Random Noise (RN) to be added to the indicated source waveform. Enter the value in volts (electrical waveforms) or Watts (optical waveforms). To apply the RN to the waveform, use the :SOURce:NOISe:STATe command.