:SOURce:PATTern

Command Syntax

:SOURceN:PATTern <pattern>

<pattern> is a token selected from those listed below.

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:PATTern?

Description

On simulated instruments, this command selects the pattern for the source waveform.

The NRZ, PAM3, PAM4, or PAM6 format is selected using the :SOURce:FORMat command.

The DATA waveform type is selected using the :SOURce:WTYPe command.

The following patterns are available using these Tokens:

Valid Command Arguments
Selection Format Description
NRZ PAM3 PAM4 PAM6
OZERo ♦       Pattern of repeating 101010…
PRBS7   ♦     37−1 pseudo-random symbol sequence (2186 symbols).
PRBS7 ♦   ♦   27−1 pseudo-random symbol sequence (127 symbols).
EPRBs7 ♦   ♦   27 pseudo-random symbol sequence (128 symbols).
PRBS9 ♦   ♦   29−1 pseudo-random symbol sequence (511 symbols).
EPRBs9 ♦   ♦   29 pseudo-random symbol sequence (512 symbols).
PRBS11 ♦   ♦   211−1 pseudo-random symbol sequence (2,047 symbols).
EPRBs11 ♦   ♦   211 pseudo-random symbol sequence (2,048 symbols).
PRBS13 ♦   ♦   213−1 pseudo-random symbol sequence (8,191 symbols).
EPRBs13 ♦   ♦   213 pseudo-random symbol sequence (8,192 symbols).
PRBS15 ♦   ♦   215−1 pseudo-random symbol sequence (32,767 symbols).
EPRBs15 ♦   ♦   215 pseudo-random symbol sequence (32,768 symbols).
LPAM4 ♦   ♦   A PAM4 linearity (160 symbols).
LPAM6       ♦ A PAM6 linearity (224 symbols).
JPA ♦       For NRZ format: JP01A. A signal with repeated sequence of two symbols that transition from level 0 to level 1.
JPB ♦       For NRZ format: JP01B. A signal with 15 pairs of symbols that transition from level 0 to level 1 followed by 16 pairs of symbols that transition from level 1 to level 0 for a total of 62 symbols.
JPC ♦       For NRZ format: JP01C. A signal with seven sets of the four symbols 0011 followed by three 0 symbols and then seven sets of the four symbols 1100 followed by three 1 symbols for a total of 62 symbols.
JPA   ♦     For PAM3 format: JP02A. A signal with repeated sequence of two symbols that transition from level 0 to level 2.
JPB   ♦     For PAM3 format: JP02B. A signal with 15 pairs of symbols that transition from level 0 to level 2 followed by 16 pairs of symbols that transition from level 2 to level 0 for a total of 62 symbols.
JPC   ♦     For PAM3 format: JP02C. A signal with seven sets of the four symbols 0022 followed by three 0 symbols and then seven sets of the four symbols 2200 followed by three 2 symbols for a total of 62 symbols.
JPA     ♦   For PAM4 format: JP03A. A signal with repeated sequence of two symbols that transition from level 0 to level 3.
JPB     ♦   For PAM4 format: JP03B. A signal with 15 pairs of symbols that transition from level 0 to level 3 followed by 16 pairs of symbols that transition from level 3 to level 0 for a total of 62 symbols.
JPC     ♦   For PAM4 format: JP03C. A signal with seven sets of the four symbols 0033 followed by three 0 symbols and then seven sets of the four symbols 3300 followed by three 3 symbols for a total of 62 symbols.
JPA       ♦ For PAM6 format: JP05A. A signal with repeated sequence of two symbols that transition from level 0 to level 5.
JPB       ♦ For PAM6 format: JP05B. A signal with 15 pairs of symbols that transition from level 0 to level 5 followed by 16 pairs of symbols that transition from level 5 to level 0 for a total of 62 symbols.
JPC       ♦ For PAM6 format: JP05C. A signal with seven sets of the four symbols 0055 followed by three 0 symbols and then seven sets of the four symbols 5500 followed by three 5 symbols for a total of 62 symbols.
K28P5 ♦       K28.5 (20 symbols)
PRBQ9     ♦   PRBS9Q (511 symbols).
PRBQ13     ♦   PRBS13Q (8,191 symbols).
PCIE     ♦   PCIe (8,768 symbols).
SSPR ♦       SSPR (32,762 symbols).
QSSPr     ♦   SSPRQ (65,535 symbols).
PRANdom ♦ ♦ ♦ ♦ A pseudo-random symbol pattern whose length is specified by the Pattern Length field (2 to 65,536 symbols) and whose initial value is indirectly specified by the Seed field.