:SOURce:OENable

Command Syntax

:SOURceN:OENable  {ON | OFF | 1 | 0}

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:OENable?

Query Response

{1 | 0}

Description

On simulated instruments, turns on or off the source waveform. On simulated instruments, to turn on or off the display of a source waveform channel, use the :CHANnel:DISPlay command.