:SOURce:JITTer:BLSTate
Command Syntax
:SOURceN:JITTer:BLSTate {ON | OFF | 1 | 0}
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:JITTer:BLSTate?
Query Response
{1 | 0}
Description
On simulated instruments, this command enables or disables bandlimiting the random jitter. When enabled, the :SOURce:JITTer:BLIMit command specified the bandwidth limit.
Example Command Sequence
:SOURce2:JITTer:BLIMit 1.485E+09 :SOURce2:JITTer:BLSTate ON