:SOURce:SSC:PHASe
Command Syntax
:SOURceN:SSC:PHASe <degrees>
<degrees> is a double.
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:SSC:PHASe?
Description
This command specifies the phase of the modulating signal. This control shifts when the modulating signal pattern (see :SOURce:SSC:PATTern) begins and ends. If the acquisition time is less than the period of the modulating signal, you can use this control to specify which portion of the modulating pattern is applied.
Example Command Sequence
:SOURce1:SSC:STATe ON :SOURce1:SSC:FREQuency 33.0E+3 :SOURce1:SSC:PHASe 0.0 :SOURce1:SSC:PERCent 0.5 :SOURce1:SSC:PPM 5.0E+3 :SOURce1:SSC:PATTern TRIangle :SOURce1:SSC:STYPe DSPRead