:SOURce:FORMat

Command Syntax

:SOURceN:FORMat {NRZ | PAM4 | PAM6}

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:FORMat?

Description

For simulated instruments, sets the type of modulation applied to the simulated input signal. Selections are NRZ (which is the default format), PAM4, and PAM6.

Example Command Sequence

:SOURce:FORMat PAM4
:SYSTem:AUToscale
*OPC?