:SOURce:SSC:PATTern

Command Syntax

:SOURceN:SSC:PATTern  {SINusoidal | TRIangle | SQUare | SAWTooth}

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:SSC:PATTern?

Description

This command specifies the shape of the modulating signal which determines the rate of change in the output symbol rate. For example, a constant rate of change from the symbol rate to the lower frequency (when using Down Spread) followed by a constant rate of change from the lower frequency back to the symbol rate is a Triangle pattern/shape.

Example Command Sequence

:SOURce1:SSC:STATe ON
:SOURce1:SSC:FREQuency 33.0E+3
:SOURce1:SSC:PHASe 0.0
:SOURce1:SSC:PERCent 0.5
:SOURce1:SSC:PPM 5.0E+3
:SOURce1:SSC:PATTern TRIangle
:SOURce1:SSC:STYPe DSPRead