:SOURce:SKEW

Command Syntax

:SOURceN:SKEW <double>

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Where <double> is the skew in seconds.

Query Syntax

:SOURce:SKEW?

Query Response

<double>

Description

On simulated instruments, specifies the amount of skew to apply to the indicated source waveform.