:SOURce:INVert
Command Syntax
:SOURceN:INVert {ON | OFF | 1 | 0}
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:INVert?
Query Response
{1 | 0}
Description
On simulated instruments, inverts the amplitude of the specified source waveform.
:SOURce2_3:AMPLitude 1.2E-1
with channel identifier 2_3 to select the connection 2 channel 3.