:SOURce:FOTWo:STATe

Command Syntax

:SOURceN:FOTWo:STATe {ON | OFF}

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:FOTWo:STATe?

Description

Sets the F/2 (Pk-Pk) jitter that is added to the simulated waveform. Use the :SOURce:FOTWo:JITTer command to enter the actual amount of jitter that is added.

The command for measuring F/2 jitter is :MEASure:JITTer:JITTer:FOVer2?.

Example Command Sequence

:SOURce5:FOTWo:JITTer 1.5E-2
:SOURce5:FOTWo:STATe ON