:SOURce:JITTer:DRN?

Query Syntax

:SOURceN:JITTer:DRN?

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Description

On simulated instruments, returns the amount of Resultant Random Noise applied to a differential source waveforms. To return the Resultant RandomJitter, use the :SOURce:JITTer:DRJ? command.