:SOURce:LEVel

Command Syntax

:SOURceN:LEVel <double>

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Where <double> is a percentage.

Query Syntax

:SOURceN:LEVel?

Query Response

<double>

Description

Creates a PAM waveform from simulated instruments that has non-linearity.

For example, in a PAM4 waveform this is accomplished by adjusting the level 1 and level 2 amplitudes. The level amplitudes are specified as a percentage between levels 0 and 3. By default, level 1 is set to 33.3% and level 2 is set to 66.7%.