:SOURce:PWIDth
Command Syntax
:SOURceN:PWIDth <seconds>
<seconds> is a double.
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:PWIDth?
Description
On simulated instruments when the Pulse function is selected (see :SOURce:FUNCtion), this command specifies the pulse width in seconds.
Example Command Sequence
:SOURce1:WTYPe FUNCtion :SOURce1:FUNCtion PULSe :SOURce1:PWIDth 1.0E-11 :SOURce1:SRATe 1.0E+9 :SOURce1:AMPLitude 0.500 :SOURce1:OFFSet 0.0