:SOURce:JITTer:STATe

Command Syntax

:SOURceN:JITTer:STATe {ON | OFF | 1 | 0}

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:JITTer:STATe?

Query Response

{1 | 0}

Description

On simulated instruments, applies or removes Random Jitter (RJ) to the source waveform. To specify the amount of RJ, use the :SOURce:JITTer:RJ command.

Example Command Sequence

:SOURce2:JITTer:RJ 1.0E-12
:SOURce2:JITTer:STATe ON