:SOURce:SRATe
Command Syntax
:SOURceN:SRATe <rate>
<rate> is a double.
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:SRATe?
Description
On simulated instruments, sets the symbol rate for the specified source waveform. The symbol rate can be any value between 50 Mb/s and 160 Gb/s. Each waveform can be set to a different symbol rate.
Example Command Sequence
:SOURce:SRATe 8.5E+9