:SOURce:NOISe:STATe
Command Syntax
:SOURceN:NOISe:STATe {ON | OFF | 1 | 0}
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:NOISe:STATe?
Query Response
{1 | 0}
Description
On simulated instruments, applies or removes Random Noise (RN) to the source waveform. To specify the amount of RN, use the :SOURce:NOISe:RN command.
Example Command Sequence
:SOURce2:NOISe:RN 1.0E-12 :SOURce2:NOISe:STATe ON