:SOURce:OFFSet
Command Syntax
:SOURceN:OFFSet <offset>
<offset> is a double.
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:OFFSet?
Description
On simulated instruments, sets the specified source waveform's offset. Enter the offset in volts for electrical channels and Watts for optical channels. To set the amplitude, use the :SOURce:AMPLitude command.
Example Command Sequence
:SOURce2:OFFSet 1.0E-3