:SOURce:FOTWo:JITTer
Command Syntax
:SOURceN:FOTWo:JITTer <jitter>
<jitter> is a double.
Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).
Query Syntax
:SOURceN:FOTWo:JITTer?
Description
Sets the amount of F/2 jitter, in unit intervals (UI), that is added to the selected simulated waveform. The default value is 10 mUI. Use the :SOURce:FOTWo:STATe command to turn apply or disable this jitter.
Example Command Sequence
:SOURce5:FOTWo:JITTer 1.5E-2 :SOURce5:FOTWo:STATe ON