:SOURce:JITTer:RJ

Command Syntax

:SOURceN:JITTer:RJ  <seconds>

<seconds> is a double.

Where N identifies a simulated instrument's specific channel in the form "<connection1-8>_<ch1-8>" (for example, SOURce4_2). With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>" (for example, SOURce3 which is the same as SOURce1_3).

Query Syntax

:SOURceN:JITTer:RJ?

Description

On simulated instruments, specifies the amount of Random Jitter (RJ) to be added to the indicated source waveform. Enter the amount of jitter in seconds. To apply the RJ to the waveform, use the :SOURce:JITTer:STATe command.

Random jitter can be applied to data and clock simulated waveform types.

Example Command Sequence

:SOURce2:JITTer:RJ 1.0E-12
:SOURce2:JITTer:STATe ON