Legacy and Compatibility Modules
Instrument
86100D
Starting with firmware release A.06.90, 86100D compatibility mode is no longer being actively tested and supported.
This section lists all the modules that are not compatible with FlexDCA's standard mode and must be run in the 86100D's Legacy mode or Compatibility mode. Use the links in this topic to learn about these modules which are no longer available.
If a module is not properly identified by the mainframe, remove the module. Click File > Exit to close FlexDCA and again to close the instrument application. Re-insert the module and finger tighten the locking screws. From the desktop, restart the instrument application.