:MEASure:JITTer:DEFine:EOPening
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:JITTer:DEFine:EOPening {PROBability | SER}
Query Syntax
:MEASure:JITTer:DEFine:EOPening?
Description
Selects the method of defining eye openings. Select either probability (PROBability) or symbol error rate (SER). The default setting is symbol error rate. For either selection, use the :MEASure:JITTer:DEFine:EOPening:PROBability child command to enter the value. This command is the same as the Probability/SER setting in the Advanced tab of the Jitter Mode Measurement Setup dialog.
Requires FlexDCA revision A.05.60 and above.