:MEASure:JITTer:DEFine:THReshold:PRESets:SELections?
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Query Syntax
:MEASure:JITTer:DEFine:THReshold:PRESets:SELections?
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for configuring the definition of thresholds for Jitter mode's measurements. Use the :MEASure:JITTer:DEFine:THReshold:PRESet command to load one of these presets.
Jitter Thresholds Presets
- CEI 56G VSR PAM4
- IEEE 802.3bs PAM4
- IEEE 802.3ck PAM4
Requires FlexDCA revision A.05.60 and above.